Würth Elektronik introduces its series of MEMS humidity sensor capacitors
Waldenburg (Germany), January 24, 2024 – Würth Elektronik is launching a very compact, cost-effective digital humidity sensor in the WSEN-HIDS series. The MEMS (Micro-Electro-Mechanical System) sensor measures with a precision of ±1.8% RH in the 20 - 80 percent relative humidity range. The DFN (Dual Flat No Leads) package for SMT assembly measures just 1.5 x 1.5 x 0.5 mm. The sensor works with a current of only 0.4 µA and can be operated with a power supply between 1.08 and 3.6 V. So it is ideally suited for distributed IoT sensor networks, such as those in smart farming applications.
The humidity sensor from Würth Elektronik uses a dielectric polymer that interacts with water molecules to adjust the permeability of the capacitor structure depending on the relative humidity of the surroundings. A temperature sensor is also included. Using the integrated analog-digital converter, the momentary temperature as well as the humidity information can be transmitted as 16-bit measurement data directly to conventional microcontrollers via an I²C interface. The heater (also included) with three selectable heating levels can be switched on temporarily as required, so the sensor works effectively even under demanding ambient conditions and the measurement is not falsified by condensation.
The Würth Elektronik humidity sensor is extremely versatile – from air conditioning equipment to data loggers in the food industry, to smart buildings, vertical farming, and other applications that require precise environmental control. It is now available from stock in any quantities. To support rapid prototyping, the sensor is part of the FeatherWing sensor and the IoT Development Kit from Würth Elektronik.
Components
Components
Würth Elektronik publishes its reference book on DC/DC converters
Continue Reading
Components
Components
Würth Elektronik in United States Embarks on New Milestone with State-of-the-Art Headquarters
Continue Reading
Components
Components
Würth Elektronik at PCIM
Continue Reading